990-91377J-001

Model List

  • Galaxy VL UPS scalable to 500 kW, 400V, start-up 5x8 (GVL0K500DS)*

  • Galaxy VL UPS 200 kW scalable to 500 kW, 400/480V, start-up 5x8 (GVL200K500DS)

  • Galaxy VL UPS 300 kW scalable to 500 kW, 400/480V, start-up 5x8 (GVL300K500DS)

  • Galaxy VL UPS 400 kW scalable to 500 kW, 400/480V, start-up 5x8 (GVL400K500DS)

  • Galaxy VL UPS 500 kW, 400/480V, start-up 5x8 (GVL500KDS)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?