990-94384-001

Configure the Display Preferences

  1. On the main menu screen, tap Configuration > Display.
    1. Set the temperature unit to Celsius or Fahrenheit.
    2. Tap the - or + to set the display brightness.
    3. Set the Alarm sound to Enable or Disable. This will enable/mute all alarm sounds.
    4. Select the wait time to activate the screen saver: 5min, 15min or 30min. Or select Never to disable the screen saver.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?