990-94384-001

Configure the Output

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > Output.
  2. Set the AC voltage ph-ph to 480VAC.
  3. Set the Frequency to 50Hz ±1.0, 50Hz ±3.0, 50Hz ±10.0, 60Hz ±1.0, 60Hz ±3.0, or 60Hz ±10.0 depending on your configuration.
  4. Tap OK to save your settings and tap the arrow symbol to go to the next page.
  5. Set the Bypass and output tolerance (%). The bypass and output tolerance range is +3% to +10%, default is +10%.
  6. Set the Overload threshold (%). The overload range is 0% to 100%, default is 75%.
  7. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?