990-94384-001

Overview of the UPS System User Interface

  1. Centralized UPS system display

    The centralized UPS system display can be used to view the status and measurements for each of the UPSs in the system and to transfer the entire UPS system between double-conversion (normal) and bypass operation. You can also configure the external disconnect devices (present/not present) and view their status. Logs and alarms are also visible in the centralized UPS system display. See Centralized UPS System Display on the I/O Cabinet – User Interface, UPS System Configuration, and Operation Procedures for the UPS System for details.

  2. Individual UPS display

    The individual UPS display shows the status and measurements for the individual UPS. Individual UPS configuration is available from this display, as well as individual UPS operation and alarms/logs. See Individual UPS Display – User Interface, Individual UPS Configuration, and Operation Procedures for the Individual UPSs for details.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?