990-94384-001

View the UPS Status Information on the Centralized UPS System Display in the I/O Cabinet


On the mimic diagram of the individual UPSs, tap on the measurements button to see the status of input, output, bypass, and battery.

Input

Example of Input Measurements on an Individual UPS

Voltage ph-ph (phase-to-phase) The present phase-to-phase input voltage.
Voltage ph-N (phase-to-neutral)* The present phase-to-neutral input voltage in volts (V).
Peak current The input peak current in amperes (A)
Current The present input current from the AC utility power source per phase in amperes (A).
Frequency The present input frequency in hertz (Hz).
Max. RMS current The present maximum RMS current in amperes (A).
Total power The present total active power input (for all three phases) in kW.
Energy The total energy consumption since the time of installation.
Power factor The ratio of the active power to apparent power.
Power The present active power (or real power) input for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

Output

Example of Output Measurements on an Individual UPS

Voltage ph-ph (phase-to-phase) The phase-to-phase output voltage at the inverter in volts (V).
Voltage ph-N (phase-to-neutral)* The phase-to-neutral output voltage at the inverter in volts (V).
Peak current The output peak current in amperes (A).
Current The present output current for each phase in amperes (A).
Frequency The present output frequency in hertz (Hz).
Load The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed.
Max. RMS current The present maximum RMS current in amperes (A).
Total power The present active total output power (for all three phases) in kilowatts (kW).
Energy The total energy supplied since the time of installation.
Neutral current* The present output neutral current in amperes (A).
Power factor The present output power factor for each phase. Power factor is the ratio of active power to apparent power.
Power The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
Crest factor The present output crest factor for each phase. The output crest factor is the ratio of the peak value of the output current to the RMS (root mean square) value.

Battery

Example of Battery Measurements on an Individual UPS

Voltage DC The present battery voltage (VDC).
Current DC The present battery current in amperes (A). A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging.
Power The present DC power being drawn from the battery, in kilowatts (kW).
Capacity The present battery charge (Ah).
Temperature Battery temperature from the connected temperature sensors in Celsius or Fahrenheit.
State of charge The present charge level of the battery as a percentage of full charge capacity.
Runtime remaining The amount of time before the batteries reach the low-voltage shutdown level.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?