990-94384-001

Centralized UPS System Display on the I/O Cabinet – User Interface

Overview of the Home Screen on the Centralized UPS System Display in the I/O Cabinet

  1. Home button - tap this button on any screen to return to the home screen.

  2. Main menu button - tap this button on any screen to access the menus. See Menu Tree for details.

  3. Mimic diagram button - tap on the gray UPS to see the mimic diagram on UPS level. See Mimic Diagram on the Centralized UPS System Display in the I/O Cabinet for details.

  4. Alarm status symbol - tap this button on any screen to access the active alarms log. See Alarm Status Symbol for details.

Mimic Diagram on the Centralized UPS System Display in the I/O Cabinet

The home screen shows the mimic diagrams for parallel systems. Tap on each UPS to see the mimic diagram on UPS level.

The mimic diagram will adapt to your system configuration – the mimic diagram shown here is just an example.

Example of Mimic Diagram on UPS Level

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

NOTE: The mimic diagram only shows one battery disconnect device BB even if more battery disconnect devices have been connected and configured for monitoring. If one or more of the monitored battery disconnect devices are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery disconnect devices are in the open position, the BB on the mimic diagram will show as open.

Menu Tree

  • Configuration*

    • System

    • Display

  • Logs

  • Communication

  • Control

  • External breakers

  • About

  • Logout

Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.

Alarm Status Symbol

The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.

Green: No alarms present in the UPS system.
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?