990-94384-001

Transfer the System Mode from Bypass Operation to Normal Operation

  1. Select Control > Transfer to normal operation.
  2. Tap OK on the confirmation screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?