990-94384-001

Export UPS Report to a USB Device

  1. Select Maintenance > UPS report.
  2. Open the front door.
  3. Insert your USB device in the USB port on the system level controller.
  4. Tap Export.
    NOTE: Do not remove the USB device until the export process has finished.
  5. Send the UPS report to Schneider Electric customer support.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?