990-94384-001

Save the UPS Settings on a USB Device

NOTE: The UPS can only accept settings that were originally saved from the same UPS. Settings saved from other UPSs cannot be reused.
  1. Tap Configuration > Save/restore.
  2. Open the front door.
  3. Insert your USB device in USB port 1 in the system level controller.
  4. Tap Save to save the present UPS settings on the USB device.
    NOTE: Do not remove the USB device until the save process has finished.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?