990-94384-001

Configure the UPS Input

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > UPS.
  2. Set the Mains configuration to Single mains .
  3. Select Autostart of the inverter if you want to enable this function. When Autostart of the inverter has been enabled, the inverter will start up automatically when input voltage returns, after a shutdown due to drained battery.
    NOTE: Autostart of the inverter is not allowed in a parallel system.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Always perform correct Lockout/Tagout before working on the UPS. A UPS with autostart enabled will automatically restart when the mains supply returns.
    Failure to follow these instructions will result in death or serious injury.
  4. Set Transformer present to No transformer present.
  5. Set Power module redundancy to N+0 or N+1.
  6. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?