990-91379F-037

连接温度/湿度传感器(可选)

可将温度/湿度传感器(AP9335T 或 AP9335TH)连接到网络管理卡。

  1. 将温度/湿度传感器连接到网络管理卡的通用 I/O 端口。
  2. 通过网络管理界面设置温度/湿度传感器,请参阅访问已配置的网络管理接口
  3. 要查看温度/湿度测量值,请点击状态 > 温度
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?