990-91262E-001

Galaxy VSUPS with Up to 5 Internal Battery StringsInstallation

20-50 kW with N+1 Power Module 400/480 V
60-100 kW 400/480 V
10-25 kW with N+1 Power Module 208 V
30-50 kW 208 V

Latest updates are available on the Schneider Electric website

5/2025

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?