990-91262E-001

Convert to a Dual Mains System

  1. Remove the static switch module.
  2. Remove the indicated plate.
  3. Remove the three single mains jumper busbars.
  4. Reinstall the plate and the static switch module.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.