990-91216D-001

Connect the Power Cables on GVSBPAR10K30H

  1. Connect the PE cables to the PE busbar.
  2. Connect the input cables from utility/mains.
  3. Connect the UPS input cables from UPS 1.
  4. Connect the UPS input cables from UPS 2.
  5. Connect the UPS output cables from UPS 1.
  6. Connect the UPS output cables from UPS 2.
  7. Connect the load cables.
  8. Fasten the cables with cable ties (provided) to the cable reliefs as shown.
QR code for this page

Was this helpful?