990-91260F-001

Galaxy VSUPS with Up to 2 Internal Battery StringsInstallation

10 kW 208 V
10-20 kW 400 V
20 kW 480 V

Latest updates are available on the Schneider Electric website

5/2025

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?