Connect the Power Cables
| NOTICE | 
|---|
| 
                      Risk of equipment damage 
                     To ensure correct load sharing in bypass operation in
                        a parallel system:
                         
                     
 Failure to follow these instructions can result in equipment damage. 
                   | 
               
- Only for TN-C/3-wire earthing system: Move the bonding busbar from position (A) to position (B) to connect the N busbar to the G/PE busbar.
 - Only for dual mains system: Remove the indicated single mains jumper cables located behind the output/bypass terminals.
 - Connect the power cables as shown:
- Connect the equipment grounding conductor/PE cables.
 - Connect the input cables.
 - Only for dual mains system: Connect the bypass cables.
 - Connect the output cables.
 
NOTE: Torque the insulated ferrules to 3.7 Nm (2.7 lb-ft / 32.7 lb-in).
 CAUTIONRisk of equipment damageCheck the fastening of the cable lugs/insulated ferrules. If the cable lugs/insulated ferrules move due to pulling on cables, the bolt/screw can become loose.Failure to follow these instructions can result in injury or equipment damage. - Reinstall the right rear plate.
 - Reinstall the left rear gland plate on the UPS.