Final Installation
|  DANGER | 
|---|
| Hazard of electric shock, explosion, or arc flash Batteries can present a risk of electric shock and high
                        short-circuit current. The following precautions must be observed
                        when working on batteries
                         
 Failure to follow these instructions will result in death or serious injury. | 
|  WARNING | 
|---|
| risk of equipment damage Wait until the system is ready to be powered up before
                        installing batteries in the system. The time duration from battery
                        installation until the UPS system is powered up must not exceed 72
                        hours or 3 days. Failure to follow these instructions can result in death, serious injury, or equipment
                        damage. | 
- Reinstall the top cover:- Tilt the top cover and slide it onto the UPS from the rear. Taps in the rear of the top cover must connect to the slots in the rear of the UPS.
- Push the top cover down in the front.
- Reinstall the screws.
 
- Remove the rear transportation bracket from the UPS.
- Only for seismic anchoring: - Install rear anchoring bracket on the UPS with the provided M8 bolts.
- Push the UPS into position so the rear anchoring bracket connects to the rear anchor.
 
- Lower the front and rear leveling feet on the UPS with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS is level.
- Only for non-seismic anchoring: Mount the front transportation bracket to the floor. The UPS can be top-heavy and tip over if not bolted to the floor. Use appropriate hardware for the floor type – the hole diameter in the front transportation bracket is ø9 mm
- Only for seismic anchoring: - Remove the front transportation bracket from the UPS.
- Install the seismic front anchoring bracket on the UPS.
- Mount the seismic front anchoring bracket on the UPS to the floor. Use appropriate hardware for the floor type – the hole diameter in the seismic front anchoring bracket is ø18 mm.
 
- Set the battery disconnect device BB to the open (OFF) position.
- Push extra battery modules (if any) into the slot. Fill the shelves from the bottom and upwards.
- Turn down the battery module handle on the extra battery modules and fasten the handle to the shelf with the provided screw.
- Connect the battery terminals to the front of the battery modules.
- Reinstall all plates and covers removed in Prepare for Installation.
- Reinstall
                  the front panel on the UPS:- Insert the two taps in the bottom of the front panel in the UPS at a tilted angle.
- Reconnect the front panel strap to the UPS.
- Close the front panel and lock with the two locking knobs.