Connect the Power Cables
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not drill or punch holes with the gland plates installed
and do not drill or punch holes in close proximity to the battery
cabinet.
Failure to follow these instructions will result in death or serious injury.
|
- Remove the gland plates.
- Drill or punch holes for cables/conduits in the rear gland
plate according to the label on the gland plate.
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHEnsure that there are no sharp edges that can damage the cables.Failure to follow these instructions will result in death or serious injury. - Install conduits (if applicable) and reinstall the gland plates.
- Route the power cables through the gland plate and connect
to the terminals:
- Connect the PE cable to the PE terminal/Connect the EGC cable to the grounding terminal.
- For installations with two hole cable lugs only, temporarily
remove the protection cover.NOTE: The protection cover must be reinstalled when the DC- cable has been connected.
- Connect the DC+ and DC- cables to the DC+ and DC- terminals.
- Connect the power cables in the UPS. If more battery cabinets
are part of the solution, connect all battery cabinets to the UPS
according to the diagram below.NOTE: If the combined short circuit current of the battery cabinets exceeds the short circuit rating of the UPS, a pull box with fuses or an external box with a battery breaker must be installed. Please contact Schneider Electric for more information and refer to the submittal drawings for your specific UPS.
- Reinstall the two transparent covers.