990-55223-001

Prepare the UPS for TN-C/480 V Solid-Grounded System

NOTE: The UPS is preconfigured for TNS earthing system.
NOTE: 480 V solid-grounded system (no neutral connection) using a bonding busbar will result in a higher leakage current.
  1. Only for TN-C/480 V solid-grounded system (no neutral connection): Install the supplied bonding busbar.

    Front View of the UPS – TN-C/480 V Solid-Grounded System (No Neutral Connection)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?