990-55223-001

Torque Specifications

Bolt size Torque for UPS Torque for Lithium-ion battery cabinet
M4 1.7 Nm (1.25 lb-ft / 15 lb-in) 1.7 Nm (1.25 lb-ft / 15 lb-in)
M5 2.2 Nm (1.62 lb-ft / 19.5 lb-in) NA
M6 5 Nm (3.69 lb-ft / 44.3 lb-in) 5 Nm (3.69 lb-ft / 44.3 lb-in)
M8 17.5 Nm (12.91 lb-ft / 154.9 lb-in)

14 Nm (10.33 lb-ft)

M10 30 Nm (22 lb-ft / 194.7 lb-in)

30 Nm (22.13 lb-ft)

M12 50 Nm (36.87 lb-ft / 442.5 lb-in)

46 Nm (33.93 lb-ft)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?