990-55222D-001

Configure the LED Strip on the Front Door

  1. Tap Configuration > General > LED strip.
  2. Select Enable UPS status via LED strip. When enabled, the LED strip on the front door of the UPS will show the UPS status. This feature is disabled by default.
  3. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.