990-55222D-001

LED Strip Lighting per UPS Operation Mode

The LED strip on the top of the front doors can show the UPS status, if enabled.

  • Green steady light means that no alarms are present for the UPS.

  • Yellow flashing light means that warning alarms are present.

  • Red flashing light means that critical alarms are present.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.