990-55222D-001

Shut Down the UPS System into Maintenance Bypass Operation

NOTE: Only operate a disconnect device when the associated disconnect device indicator lamp is illuminated.
  1. Shut down the UPS system using Guided sequences:
    • For a single UPS system: Select Control > Guided sequences > Shut down UPS system and follow the steps which appear on the display.
    • For a parallel UPS system: Select Control > Guided sequences > Shut down a UPS in a parallel system and follow the steps which appear on the display.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.