990-55222D-001

Restore the UPS Settings from a USB Device

NOTE: The UPS can only accept settings that were originally saved from the same UPS. Settings saved from other UPSs cannot be reused.
Settings can only be restored when the UPS is in maintenance bypass operation or off mode.
  1. Tap Control > Guided sequences > Shut down UPS system or Control > Guided sequences > Shut down a UPS in a parallel system, and follow the steps which appear on the display.
    NOTE: Do not open the unit input disconnect device UIB at the end of the shutdown sequence as this will turn off the power to the display.
  2. Select Configuration > Save/restore.
  3. Open the front door.
  4. Insert your USB device in USB port 1 in the system level controller.
  5. Tap Restore to implement saved UPS settings from the USB device. Wait for the system level controller to reboot automatically.
    NOTE: Do not remove the USB device until the restore process has finished.
  6. Select Control > Guided sequences > Start up UPS system or Control > Guided sequences > Start up a UPS in a parallel system, and follow the steps which appear on the display.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.