990-55222D-001

Start Up the UPS System from Maintenance Bypass Operation

NOTE: Only operate a disconnect device when the associated disconnect device indicator lamp is illuminated.
  1. If open, close the unit input disconnect device UIB.
    The display turns on. The rebooting sequence lasts approximately 3 minutes.
  2. Start up the UPS system using Guided sequences:
    • For a single UPS system: Select Control > Guided sequences > Start up UPS system and follow the steps which appear on the display.
    • For a parallel UPS system: Select Control > Guided sequences > Start up a UPS in a parallel system and follow the steps which appear on the display.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.