990-55222D-001

Tests

The UPS system can perform the following tests to ensure correct performance of the system:

  1. Tap Maintenance. Then tap the button of the function to start the test of the function.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.