990-55222D-001

Start Up the UPS System from Maintenance Bypass Operation with an Inoperable Display

NOTE: If the display is operable, always go to Control > Guided sequences and follow the steps on the display to start up the UPS.
  1. If open, close the unit input disconnect device UIB.
  2. Close the static switch input disconnect device SSIB (if present).
  3. Close the bypass backfeed disconnect device BF2 (if present).
  4. Close the battery disconnect device(s).
  5. Press and hold the inverter ON button on the system level controller for 5 seconds. This will turn on the inverter and transfer the UPS to inverter operation (eConversion or double-conversion mode). Check that the inverter LED is green on the system level controller. See Status LED Lighting per UPS Operation Mode.
  6. Close the unit output disconnect device UOB.
  7. In a parallel system: Repeat step 1 to 6 for the other UPSs in the parallel system.
  8. In a parallel system: Close the system isolation disconnect device SIB (if present).
  9. Open the maintenance bypass disconnect device MBB.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.