GEX75737

Service Entry Requirements

USA and Mexico

Switches not factory bonded are shipped suitable for use as service equipment.

Switches that are shipped from the factory with a bonded neutral are suitable for use as service equipment.

For use on other applications, the bonding screw should be removed.

Enclosure must be grounded.

Devices require line side barriers.

Enclosure must be bonded via a bonding screw or jumper; bonding the insulated neutral to the enclosure.

Canada

Switches that are shipped from the factory with a bonded insulated neutral are suitable for use as service equipment.

Canada factory bonded insulated neutral can be unbonded and used for other applications other than the service entrance.

NOTE: Review electrical code CSA C22.1 Article 6-212 for wiring requirements.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.