GEX75737

Replacing the Viewing Window 30–200 A

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or NOM-029-STPS.
  • This equipment must only be Installed and serviced by qualified electrical personnel.
  • Never operate energized switch with door open.
  • Turn off switch before removing or Installing fuses or making load side connections.
  • Always use a properly rated voltage sensing device at all line and load fuse clips to confirm switch Is off.
  • Turn off power supplying switch before doing any other work on or Inside switch.
  • Do not use renewable link fuses In fused switches.
Failure to follow these instructions will result in death or serious injury.

Unhook Snap from Cover

Snaps in Place

  1. Turn off power supplying the switch before performing any work on or inside the switch.

  2. Open the switch blades by moving the operating handle to the OFF (O) position.

  3. Lock out or tag the switch, per local procedures.

  4. Open the enclosure door.

  5. Always use a properly rated voltage sensing device at all line and load-side lugs (terminals) to confirm power is off.

  6. From inside of front cover use a screw driver to unhook snap from cover and push window out (do on all snap locations). See Figure 6.

  7. Center new window in the opening.

  8. Apply equal force on window to snap into place.

  9. Confirm that snaps are properly engaged. See Figure 7.

  10. Close the door. Complete any lock out tag out procedures required. Energize, as required.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.