GEX75737

Class R Rejection Clip Kits

It is required to obtain full rating of Class R fuses, without clips the system rating is reduced to 10 kAIC, since switch can have Class H or Class K still installed.

Ampere Rating

Voltage Rating

Kit Catalog

30

240 V

RFK03L

30

600 V

RFK03H

30 *

RFK06

30 *

RFK06

60

240 V

RFK03H

60

600 V

RFK06H

100

240 V and 600 V

RFK10

200

RFK1020

400

RFK4060

600

RFK4060

  1. Turn OFF (O) all power supplying switch and follow lockout/tag-out procedures.

    NOTE: Each fuse has rejection provisions on one end only. Ears on adapter fit into small slots in molded base, near fuse clip (A) on line end.
  2. Push fuse adapter (B) firmly into slot in molded base (C) with circular portion going into slot in either side of fuse clip. Make sure ears (D) of adapter snap into base so adapter cannot be removed.

  3. Refer to the Class R Rejection Clip Kits for additional information.

NOTE: Class J fuses require moving of the Load Base Assembly to holes marked on the devices. 600 A also requires Kit: H600J.

Moving the Load Base Assembly

  1. Remove two mounting screws (can be used for remounting) that have load base located for Type H, K and R fuses.

  2. Align load base for mounting location for Type J fuses.

  3. Use screws to reattach load base. Refer to the table below for the appropriate torque value.

Amperage

Torque

30 A

20–30 lb–in. (2.26–3.39 N•m)

60 A

25–35 lb–in. (2.82–3.95 N•m)

100 A

200 A

30–50 lb–in. (3.39–5.65 N•m)

400 A

55–60 lb–in. (6.21–6.78 N•m)

600 A

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.