80459-641-04

Ground Bus Splicing

NOTE: The MCC horizontal ground bus is located at the bottom of each MCC structure. It can be accessed by removing the bottom horizontal wireway cover or other bottom located cover on the structure. The ground bus splice plate is located on the right end of the ground bus in each shipping split.

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
Failure to follow these instructions will result in death or serious injury.

Type 1, Type 12, and Type 3R

To splice the ground bus:

  1. Turn off all power supplying this equipment before working on or inside the equipment, and follow lockout/tagout procedures. Always use a properly rated voltage sensing device to confirm the power is off.

  2. Remove ground bar bolts from the right and left sections.

  3. Slide the ground splice bar into the right section, aligning the mounting holes (see ).

    Ground Bar Bolt Replaced

  4. Replace the ground bar bolts (see ) in the right and left sections. Torque both bolts to 60–75 lb-in. (6.75–8.44 N•m).

  5. Replace all covers and barriers, and close all doors.

Bottom-Feed ArcBlok Main Sections–1200 A

To splice the ground bus, follow these steps:

  1. Remove the cable vault front cover to access the ground bus assembly.

  2. Remove the ground bar bolts in the cable vault and in the adjacent MCC section.

  3. Slide the ground splice bar into the right section, aligning the mounting holes.

  4. Replace the ground bar bolts (see Ground Bar Bolt Replaced) in the right and left sections.

  5. Torque the ground bar bolts to 60–75 lb-in. (6.75–8.44 N•m).

  6. Place the ground closing plates into position to seal the cable vault (see Location of Ground Closing Plates). Slide the closing plates against the ground bar where the bar passes into the next section. Where there is not a splice to an adjacent section, completely cover the unused ground bus opening with the closing plate.

    Location of Ground Closing Plates

  7. Replace all covers and barriers, and close all doors.

Bottom-Feed ArcBlok Main Sections–1600, 2000, and 2500 A

  1. Remove the cable vault front cover to access the ground bus assembly.

  2. For splicing to left adjacent section (if applicable):

    • Remove the bolts for the ground splice bar located on the left-side of the cable vault and the ground splice bar located on the right-side of the left adjacent section. (see Removing Bolts for Ground Splice Bar).

      Removing Bolts for Ground Splice Bar

    • Discard the ground splice bar on the right side of the left adjacent section.

    • Loosen the ground closing plate hardware on the left side of the cable vault and slide the closing plate forward to reveal open slot in cable vault.

    • Slide the ground splice bar located inside the cable vault to the left so that it aligns with the mounting hole of the ground bus in the left adjacent section.

    • Re-install one ground splice bar bolt in both sections, (see Re-install Ground Splice Bar Bolt).

      Re-install Ground Splice Bar Bolt

    • Torque the ground splice bar bolts to 60–75 lb-in. (6.75–8.44 N•m).

    • Slide the closing plate against the ground splice bar and tighten the ground closing plate hardware.

  3. For splicing to right adjacent section (if applicable):

    • Remove the bolts for the ground splice bar located on the right-side of the cable vault.

    • If applicable, remove the bolts for the ground splice bar located on the left-side of the right adjacent section and discard the ground splice bar.

    • Loosen the ground closing plate hardware on the right side of the cable vault and slide the closing plate forward to reveal open slot in cable vault.

    • Slide the ground splice bar located inside the cable vault to the right so that it aligns with the mounting hole of the ground bus in the right adjacent section.

    • Re-install one ground splice bar bolt in both sections.

    • Torque the ground splice bar bolts to 60–75 lb-in. (6.75–8.44 N•m).

    • Slide the closing plate against the ground splice bar and tighten the ground closing plate hardware.

  4. Replace all covers and barriers and close all doors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.