80459-641-04

Modifying Fuse Clip Locations

DANGER
Hazard of Electric Shock, Explosion, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment and follow lockout/tagout procedures before working on or inside equipment.
  • Never operate energized switch with door open.
  • Turn off switch before removing or installing fuses or making load side connections.
  • Always use a properly rated voltage sensing device at all line and load fuse clips to confirm switch is off.
  • Turn off all power supplying switch before doing any other work on or inside switch.
  • Do not use renewable link fuses in fused switches.
Failure to follow these instructions will result in death or serious injury.

Install 30 and 60 A fuse bases for the proper fuse size and class and maximum voltage in Size 1 and 2 starter units. The base pan of the disconnect switch has five sets of mounting holes for this purpose. The lower fuse base is installed in the proper mounting holes at the factory (see Size 1 and 2 Fuse Clip Locations). Additional clips and bases may be required if changing fuse class.

Size 1 and 2 Fuse Clip Locations

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.