80459-641-04

Introduction

This bulletin contains instructions on handling, installing, maintaining, and modifying, a new Model 6 Motor Control Center (MCC).

Additional information related to expanding a Model 6 MCC, retrofit of various components in a Model 6 MCC, and other related topics can be found in instruction bulletin 80459-641-01, Model 6 Motor Control Centers.

Arc-Rated MCC

The arc-rated Model 6 MCC has a device-limited arc resistant rating up to 65 kA at 600 V. The rating requires specific up-stream circuit protection. For information on up-stream protective device requirements, see instruction bulletin 80459-641-01, Model 6 Motor Control Centers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.