80459-641-04

Installing the MCC

This section explains how to locate, install, and join Model 6 MCC enclosures, and how to splice power and ground bus. Refer to MCC front elevation drawings supplied by Schneider Electric for location/placement of shipping splits/sections within each MCC line-up.

Locating the MCC

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, CSA Z462, or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • When moving MCC sections, follow the instructions in Handling the MCC. The MCC has a high center of gravity, which may cause it to tilt.
  • MCC structures must be secured to the mounting surface. Follow instructions in Securing Structures to the Floor.
Failure to follow these instructions will result in death or serious injury.

MCCs are designed for use in non-hazardous locations. Choose a location for installation that is well ventilated and free from excess humidity, dust, and dirt. The temperature of the area should be no less than 0°C (32°F) and no greater than 40°C (104°F). Protect the MCC from the entrance of water or any moisture. If necessary, protect the MCC from condensation by ordering internal space heaters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.