80459-641-04

Thermal Overload Unit Selection

This section identifies the thermal overload units needed for the starters specified in an order. Tables are based on motor full-load amps and provide the catalog number for the appropriate thermal units to be used at that current rating.

Melting Alloy Overload Selection Tables for Combination Starter Units

Size 1

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

0.56–0.63

B 0.81

4.12–4.70

B 6.90

0.64–0.68

B 0.92

4.71–5.21

B 7.70

0.69–0.77

B 1.03

5.22–5.53

B 8.20

0.78–0.85

B 1.16

5.54–6.17

B 9.10

0.86–0.97

B 1.30

6.18–7.02

B 10.2

0.98–1.09

B 1.45

7.03–7.92

B 11.5

1.10–1.21

B 1.67

7.93–8.61

B 12.8

1.22–1.33

B 1.88

8.62–9.17

B 14

1.34–1.53

B 2.10

9.18–10.0

B 15.5

1.54–1.73

B 2.40

10.1–11.0

B 17.5

1.74–1.89

B 2.65

11.1–11.8

B 19.5

1.90–2.17

B 3.00

11.9–13.5

B 22

2.18–2.53

B 3.30

13.6–15.3

B 25

2.54–2.87

B 3.70

15.4–17.4

B 28

2.88–3.22

B 4.15

17.5–19.4

B 32

3.23–3.49

B 4.85

19.5–22.2

B 36

3.50–3.85

B 5.50

22.3–25.1

B 40

3.86–4.11

B 6.25

25.2–27.0

B 45

Size 2

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

3.94–4.45

B 6.90

14.0–15.8

B 25

4.46–4.97

B 7.70

15.9–17.9

B 28

4.98–5.28

B 8.20

18.0–19.9

B 32

5.29–5.97

B 9.10

20.0–22.8

B 36

5.98–6.89

B 10.2

22.9–25.4

B 40

6.90–7.92

B 11.5

25.5–28.9

B 45

7.93–8.71

B 12.8

29.0–30.8

B 50

8.72–9.27

B 14.0

30.9–32.5

B 56

9.28–10.2

B 15.5

32.6–34.9

B 62

10.3–11.4

B 17.5

35.0–39.7

B 70

11.5–12.3

B 19.5

39.8–44.7

B 79

12.4–13.9

B 22

Size 3

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

14.0–14.9

CC 20.9

36.9–39.8

CC 59.4

15.0–16.2

CC 22.8

39.9–42.3

CC 64.3

16.3–17.2

CC 24.6

42.4–45.7

CC 68.5

17.3–18.7

CC 26.3

45.8–49.2

CC 74.6

18.8–20.2

CC 28.8

49.3–52.8

CC 81.5

20.3–21.7

CC 31.0

52.9–56.8

CC 87.7

21.8–23.3

CC 33.3

56.9–61.2

CC 94.0

23.4–25.2

CC 36.4

61.3–66.1

CC 103

25.3–27.1

CC 39.6

66.2–71.2

CC 112

27.2–29.4

CC 42.7

71.3–76.7

CC 121

29.5–31.6

CC 46.6

76.8–82.9

CC 132

31.7–34.0

CC 50.1

83.0–90.0

CC 143

34.1–36.8

CC 54.5

Size 4

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

44.0–46.8

CC 64.3

73.0–78.1

CC 112

46.9–50.6

CC 68.5

78.2–83.9

CC 121

50.7–54.5

CC 74.6

84.0–91.1

CC 132

54.6–58.4

CC 81.5

91.2–97.5

CC 143

58.5–62.9

CC 87.7

97.6–104

CC 156

63.0–67.7

CC 94.0

105–113

CC 167

67.8–72.9

CC 103

114–133

CC 180

Size 5 with CT Type Overloads

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

40.8–45.5

B 1.03

115–128

B 3.00

45.6–49.9

B 1.16

129–140

B 3.30

51.0–57.5

B 1.30

141–160

B 3.70

57.6–65.9

B 1.45

161–193

B 4.15

66.0–73.1

B 1.67

194–209

B 4.85

73.2–81.5

B 1.88

210–232

B 5.50

81.6–92.3

B 2.10

233–248

B 6.25

92.4–104

B 2.40

249–266

B 6.90

105–114

B 2.65

Size 6

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

133–148

B 1.30

272–308

B 2.65

149–174

B 1.45

309–348

B 3.00

175–195

B 1.67

349–397

B 3.30

196–219

B 1.88

398–429

B 3.70

220–239

B 2.10

430–495

B 4.15

240–271

B 2.40

496–520

B 4.85

Melting Alloy Overload Selection Tables for Part Winding Combination Starter Units

Size 1

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

1.12–1.27

B 0.81

8.24–9.41

B 6.90

1.28–1.37

B 0.92

9.42–10.43

B 7.70

1.38–1.55

B 1.30

10.44–11.07

B 8.20

1.56–1.71

B 1.16

11.08–12.35

B 9.10

1.72–1.95

B 1.30

12.36–14.05

B 10.2

1.96–2.19

B 1.45

14.06–15.85

B 11.5

2.20–2.43

B 1.67

15.86–17.23

B 12.8

2.44–2.67

B 1.88

17.24–18.35

B 14

2.68–3.07

B 2.10

18.36–20.1

B 15.5

3.08–3.47

B 2.40

20.2–22.1

B 17.5

3.48–3.79

B 2.65

22.2–23.7

B 19.5

3.80–4.35

B 3.00

23.8–27.1

B 22

4.36–5.07

B 3.30

27.2–30.7

B 25

5.08–5.75

B 3.70

30.8–34.9

B 28

5.76–6.45

B 4.15

35.0–38.9

B 32

6.46–6.99

B 4.85

39.0–44.5

B 36

7.00–7.71

B 5.50

44.6–50.3

B 40

7.72–8.23

B 6.25

50.4–54.0

B 45

Size 2

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

7.88–8.91

B 6.90

24.8–27.9

B 22

8.92–9.95

B 7.70

28.0–31.7

B 25

9.96–10.57

B 8.20

31.8–35.9

B 28

10.58–11.95

B 9.10

36.0–39.9

B 32

11.96–13.79

B 10.2

40.0–45.7

B 36

13.80–15.85

B 11.5

45.8–50.9

B 40

15.86–17.43

B 12.8

51.0–61.7

B 45

17.44–18.55

B 14.0

61.8–65.1

B 50

18.56–20.5

B 15.5

65.2–69.9

B 56

20.6–22.9

B 17.5

70.0–79.5

B 62

23.0–24.7

B 19.5

79.6–89.4

B 70

Size 3

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

28.0–29.9

CC 20.9

73.8–79.7

CC 59.4

30.0–32.5

CC 22.8

79.8–84.7

CC 64.3

32.6–34.5

CC 24.6

84.8–91.5

CC 68.5

34.6–37.5

CC 26.3

91.6–98.5

CC 74.6

37.6–40.5

CC 28.8

98.6–105.7

CC 81.5

40.6–43.5

CC 31.0

105.8–113.7

CC 87.7

43.6–46.7

CC 33.3

113.8–122.5

CC 94.0

46.8–50.5

CC 36.4

122.6–132.3

CC 103

50.6–54.3

CC 39.6

132.4–142.5

CC 112

54.4–58.9

CC 42.7

142.6–153.5

CC 121

59.0–63.3

CC 46.6

153.6–165.9

CC 132

63.4–68.1

CC 50.1

166.0–180.0

CC 143

68.2–73.7

CC 54.5

Size 4

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

105–112

CC 74.6

170–181

CC 132

113–122

CC 81.5

182–195

CC 143

123–131

CC 87.7

196–209

CC 156

132–142

CC 94.0

210–227

CC 167

143–153

CC 103

228–247

CC 180

154–157

CC 112

248–266

CC 196

158–169

CC 121

Size 5 with CT Type Overloads

Motor Full‑Load Current (A)

Thermal Unit Number

Motor Full‑Load Current (A)

Thermal Unit Number

81.6–91.1

B 1.03

230–257

B 3.00

91.2–101

B 1.16

258-281

B 3.30

102–115

B 1.30

282–321

B 3.70

116–131

B 1.45

322–387

B 4.15

132–146

B 1.67

388–419

B 4.35

147–163

B 1.84

420–465

B 5.60

164–184

B 2.10

466–497

B 6.25

185–209

B 2.40

496–532

B 6.90

210–229

B 2.65

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.