80459-641-04

Receiving, Handling, and Storing the MCC

See requirements for Moisture Contamination Avoidance and Mitigation for additional information on receiving and inspecting electrical equipment.

Most MCCs are shipped in one-, two-, or three-section shipping blocks with the MCC sections laying on their side on a pallet. At the customer’s request, MCCs can be shipped in a standing position. Some heavier MCC sections are only shipped in a standing position.

Receiving the MCC

Inspect the MCC for damage as soon as it is received. Delivery of the equipment to a carrier at any of the Schneider Electric plants or other shipping point constitutes delivery to the purchaser. Title and all risk of loss or damage in transit shall pass to the purchaser at that time. Refer to the Schneider Electric Conditions of Sale for more details. All claims for loss and damage must be made by the purchaser to the carrier.

If the packaging material is removed, replace it for protection until the MCC is installed.

Handling the MCC

WARNING
tip over Hazard
  • Before installing or uninstalling this product, read and follow the product instructions for handling.
  • This product has a high center of gravity. Use properly rated lifting equipment to move the product and prevent tipping.
  • During the installation, secure the product to the mounting surface. Follow instructions in Securing Structures to the Floor.
  • This product must be handled and installed only by qualified personnel.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Equipment Needed

Adequate equipment, such as a fork truck, crane, or rods and pipe rollers, must be available for handling MCCs. Approximate MCC Shipping Weights lists the approximate shipping weights of sections equipped with typical units. For more exact shipping weights for the particular set-up, contact the MCC Technical Assistance Group at 800-634-2003.

Approximate MCC Shipping Weights

Enclosure Type

Depth

One Section

Two Sections

Three Sections

1, 1A, 12

15 in. (381 mm)

600 lb (272 kg)

1200 lb (544 kg)

1800 lb (816 kg)

3R Non-Walk-In

15 in. (381 mm)
(26.6 in. / 676 mm overall)

900 lb (408 kg)

1800 lb (816 kg)

2700 lb (1225 kg)

1, 1A, 12

20 in. (508 mm)

750 lb (340 kg)

1500 lb (680 kg)

2250 lb (1021 kg)

3R Non-Walk-In

20 in. (508 mm)
(31.6 in. / 803 mm overall)

1050 lb (476 kg)

2100 lb (953 kg)

3150 lb (1429 kg)

18-Pulse Drive

50 in. W (1270 mm)

20 in. (508 mm)

N/A

2107 lb (956 kg)

65 in. W (1651 mm)

2816 lb (1277 kg)

Moving the MCC

WARNING
tip over hazard
While moving the MCC:
  • Follow all manufacturer-specified instructions and precautions when moving heavy equipment.
  • Verify that the moving equipment is rated to handle the weight.
  • Fork trucks, when available, provide a convenient method of moving MCCs. Use extended forks when lifting 42 in. (1067 mm), minimum.
  • Secure the load to the lifting equipment before moving.
  • When removing an MCC from a shipping pallet, carefully balance and secure it using a properly rated strap.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
handling and lifting hazard
  • Product must only be lifted by qualified personnel.
  • Keep area below equipment clear of any personnel or property.
  • Inspect lifting angle for any damage. Do not lift if damage is found.
  • Select rigging lengths to compensate for unequal weight distribution.
  • Limit sling angle to less than 45° maximum angle between the vertical and lifting cables (see Proper Use of Sling to Lift MCCs).
  • Do not pass ropes, cables or slings through lifting angle holes. Use properly rated hooks or shackles.
  • Use only properly rated lifting equipment to lift product.
  • Lift from upright position only. Keep lifting force vertical.
  • Do not attempt to lift or attach lifting means to sections equipped with pull boxes.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Proper Use of Sling to Lift MCCs

The lifting angle(s) on standard Model 6 MCCs may be removed and discarded. On arc rated MCCs, MCC sections with ArcBlok main breakers, or MCCs with ventilated top plates, the lifting angle(s) must be removed. To prevent entrance of foreign materials, replace all hardware that secured the lifting angle.

Plug-In Units

Some MCC units can weigh up to 200 pounds and require two or more persons or special handling equipment. Lift only by supporting bottom and/or side panels of the unit. Refer to instruction bulletin 80459-641-01, Model 6 Motor Control Centers, for details on unit installation and removal and additional lifting information.

Storing the MCC

NOTICE
HAZARD OF MOISTURE INGRESS AND CORROSION
Never store MCCs outdoors. Outdoor storage is inadequate, even with the protection of a tarpaulin.
Failure to follow these instructions can result in equipment damage.

If the MCC cannot be placed into service upon receipt, store it in a clean, dry, ventilated building free from temperature extremes.

See requirements for Moisture Contamination Avoidance and Mitigation for additional information on storage of electrical equipment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.