LVPED508016EN–03

Standard End-User Preventive Maintenance Program

Definition

The Standard end-user preventive maintenance program can be carried out by:

  • Trained and qualified maintenance services provider personnel.

  • Schneider Electric field service representatives.

The Standard end-user preventive maintenance program includes the Basic end-user preventive maintenance program.

The Standard end-user preventive maintenance program comprises:

  • Extended visual inspection.

  • Extended function checks.

  • Part and system servicing (cleaning, greasing).

  • Part replacement (based on time intervals or number of units of use).

The Standard end-user preventive maintenance program must be performed every two years in the case of normal operating conditions. Refer to the recommended frequency for the Standard end-user maintenance program for other cases.

Procedures

The Standard end-user procedures are described in detail in MasterPact NT/NW - Basic and Standard End-User Maintenance Procedures for IEC Devices.

Part

Procedure title

Procedure name

Mechanism

Check the MCH gear motor charging time at 0.85 Un

Mechanism NIII_2_1

Check the general condition of the mechanism

Mechanism NIII_2_2

Check the number of device operating cycles

Mechanism NIII_2_3

Breaking unit (arc chutes + contacts)

Check the condition of the breaking unit

Breaking Unit NIII_2_1

Check mounting of arc chutes and filter cleanliness

Breaking Unit NIII_2_2

Auxiliaries

Check operation of indication contacts (OF, PF)

Auxiliaries NIII_2_1

Check closing operation with XF closing voltage release at 0.85 Un

Auxiliaries NIII_2_2

Check opening operation with MX opening voltage release at 0.70 Un

Auxiliaries NIII_2_3

Check closing and opening operations with MN undervoltage release

Auxiliaries NIII_2_4

Check time delay of MNR delayed undervoltage release

Auxiliaries NIII_2_5

Control unit

Check overcurrent protection

Control Unit NIII_2_1

Save protection settings, reports, and event logs (MicroLogic P and H)

Control Unit NIII_2_3

Chassis

Clean chassis and check presence of grease on chassis

Chassis NIII_2_1

Check disconnecting contact clusters

Chassis NIII_2_2

Check operation of safety shutters

Chassis NIII_2_3

Check operation of CD, CT, CE position contacts and EF auxiliary contacts

Chassis NIII_2_4

Power connections

Check connection system

Power Connections NIII_2_1

Tools

Performing the procedures of the maintenance program requires the following:

Time Required

In addition to the Basic end-user maintenance program, the average time required for experienced, trained, and qualified maintenance personnel to perform this maintenance program is as follows:

  • 45 minutes for a fixed device with all accessories installed

  • 1 hour for a drawout device with all accessories installed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?