DUG_Iconic Connected Dimmer_PDL-00

Changing device protocol

The communication protocol of the device can be changed from Zigbee to Bluetooth and Bluetooth to Zigbee.

Reset the device before changing device protocol. Refer resetting the device.

Short press the push-button 3 times and then long press the push-button once (> 20s).

Red led flash rapidly indicating commence of protocol change.

On successful change in protocol:

  • Zigbee to Bluetooth - No colour indication, white back light only.

  • Bluetooth to Zigbee - Flashing Amber LED (Indicating that device is in pairing mode), if pairing is not completed will become solid Amber

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?