DUG_Iconic Connected Dimmer_PDL-00

Removing the device

Using the Wiser app, you can remove a device from the device list.
  1. On the Home page, tap All devices > Iconic Dimmer.
  2. Tap to display more details.
  3. Tap Remove device (A) and select any of the following:
    • Disconnect: to remove the device.
    • Disconnect & Erase Data: to remove the device and erase data.
    TIP: On the Home page, tap and hold the Iconic Dimmer to remove the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?