DUG_Iconic Connected Dimmer_PDL-00

Creating a schedule

Using a schedule, you can control and trigger the dimmer. The system will follow the active schedule once it has been set. You can create or modify schedules at any time.
  1. On the Home page, tap All devices > Iconic Dimmer.
  2. Tap Schedule > Add schedule to add a schedule.
  3. Set the time (A).
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification when the task is executed at the time of schedule.
  7. In the Iconic Dimmer section, drag the sliding bar (E) to do one of the following:
    • 100%: turns on the dimmer with maximum brightness on the scheduled time.
    • Off: turns off the dimmer on the scheduled time.
    • Drag the sliding bar anywhere in between to turn on the dimmer with a set brightness level on the scheduled time

  8. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?