DUG_Iconic Connected Dimmer_PDL-00

LED Indicator Settings

You can select the LED indicator mode for easy identification of the device status.

On the Settings page, tap LED Indicator Settings and select any of the following:

- Always On: LED on the device is always turned on.

- On with Timeout but as Locator: LED glow in lesser brightness after the time out.

- On with Timeout: After inactive period LED turns off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?