DUG_Iconic Connected Dimmer_PDL-00

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • It is illegal for persons other than an appropriately licensed electrical contractors or other persons authorised by legislation to work on the fixed wiring of any electrical installation.
  • To comply with all safety standards, the device must be used only for the purpose described in this instruction and must be installed in accordance with the wiring rules and regulation in the location where it is installed.
  • Lock out and tag the input circuit before accessing the wiring connections.
  • The Locking Bar on the grids must be set to the Closed position to ensure that the device cannot be removed during normal operation.
  • There are no user serviceable parts inside the device.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE HAZARD (LOAD AND OPERATION)
  • Operation of the device at elevated temperatures or voltages outside of specification (240 V a.c. and 25 °C) may cause the over-temperature protection circuitry to operate.
  • Reduce the size of the connected load or use a different brand of fan to prevent recurrence.
  • Do not operate the product for prolonged periods in extreme conditions.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?