DUG_Iconic Connected Dimmer_PDL-00

Using the device

The Control Panel allows you to switch the Dimmer on/off, increase/decrease the brightness and control various settings.

On the Home page, tap All devices > Iconic Dimmer to access the control panel.

On the control panel page, you can see the following:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?