DUG_Iconic Connected Dimmer_PDL-00

Dimming Range

You can restrict the minimum and maximum brightness of the load connected to the device. This is done to avoid flickering and switching off the LED.

On the Setting page, tap Dimming Range and do either or both of the following:

Minimum Brightness: drag the sliding bar to restrict the minimum brightness.

TIP: If you set the minimum brightness to the right most position on this sliding bar, then the load glows at the minimum brightness even if you drag the sliding bar to the lowest value in the control panel.

Maximum Brightness: drag the sliding bar to restrict the maximum brightness.

TIP: If you set the maximum brightness to the left most position on this sliding bar, then the load glows at the maximum brightness even if you drag the sliding bar to the highest value in the control panel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?