7EN72-0197-01

Power quality: ION meters and EN50160:2010Technical Note

This technical note summarizes the EN50160 data and statistics measured by the PowerLogic™ ION™ meters that monitor compliance to the EN51060:2010 standard, and includes references to the applicable parts of IEC 61000-4-30. This documentation assumes that you have an advanced understanding of ION architecture, EN50160:2010, IEC 61000-4-30 standard, and the power system that your meter is connected to.

02/2017

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?