Commissioning Rules
The commissioning rules are applicable to the gateway webpages.
Rule COM1: Use the Manual Channel Selection mode in concentrated wireless architecture.
In concentrated wireless architecture, the PowerTag systems interfere between themselves. Therefore, the channel must be set according to the wireless channel assignment plan in Manual Channel Selection mode.
Rule COM2: Configure the wireless channel before the wireless devices discovery.
-
Set the channel value before pairing the wireless devices to save time.
-
In case of wireless channel modification after pairing, the PowerTag system will need several minutes or hours to recover wireless communication.
Rule COM3: Save the PowerTag Link gateway configuration.
Generate a backup file of the PowerTag Link gateway configuration at the end of the commissioning.
It is possible to replace a defective PowerTag Link gateway by a new one without load power outage if a backup file was previously generated and saved.
Without this backup file, it is mandatory to restart all the wireless devices (and interrupt the associated supply load) to replace the PowerTag Link gateway.
It is recommended to generate and save these backup files, especially when the PowerTag Link gateway is to be installed with high level of continuity of service and critical supply load.