Wireless Channel Assignment Plan Rules
Rule WCAP1: Assign non-contiguous channels in a panel.
Follow the rules to assign non-contiguous channels in a panel:
-
Do not use the same channel for several gateways inside an enclosure.
-
Do not use contiguous channel for adjacent gateway inside an enclosure.
-
Prefer to use non-contiguous channels inside an enclosure.
Rule WCAP2: Privilege channel not overlapped by another radio frequency signal.
Follow the rules to avoid overlapping of privilege channel by another radio frequency signal:
-
Do not use the privileged channels if they are known before the design plan of wireless channel assignment plan design.
-
Check the behavior of the PowerTag system during commissioning in the end user site.
Rule WCAP3: Reserve channels for future evolution.
Follow the rules to reserve the channels for future evolution::
-
Two channels, if the density will be up to 1500 wireless devices in a radius of 20 meters.
-
One additional dedicated channel, if any third-party radio frequency network is to be added for other wireless system.
Rule WCAP4: Define the available channels.
Follow the rules to define the available channels:
-
Use all the available channels to balance the gateways and their paired wireless devices.
Available channels = 16 - overlapped channels - reserved channels
-
Use the channels uniformly.
-
Priority 1: Maximize the distance between the gateway using the same channel.
-
Priority 2: Maximize the distance between the gateway using channel X and adjacent channels – Channel X-1 and X+1.
Rule WCAP5: Define two wireless communication periods according to the wireless devices density.
Follow the rules to define the values of two wireless communication periods:
-
Set the same wireless communication periods for all gateways of the zone.
-
Up to 400 wireless devices in a radius of 20 meters, set the wireless communication periods to 30 seconds minimum.
-
Up to 600 wireless devices in a radius of 20 meters, set the wireless communication periods to 60 seconds minimum.
-
More than 600 wireless devices in a radius of 20 meters, contact your Schneider Electric representative.
|
Number of wireless devices in a radius of 20 m
|
Minimum wireless communication period recommended (Twireless comm) |
|---|---|
|
Up to 100 |
5 s |
|
Up to 200 |
10 s |
|
Up to 400 |
30 s |
|
Up to 600 |
60 s |
Twireless comm is the wireless communication period defined for the type of device in the gateway configuration.