Enclosure Implementation Rules
Rule SW1: Mount the gateway in the center of the switchboard.
Reduce the distance between the gateway and the wireless devices to avoid wireless communication disturbances.
Rule SW2: Supply the wireless devices and gateway as upstream as possible in the switchboard.
To secure the power supply of a gateway, PowerTag Link display, PowerTag control modules, and HeatTag sensor, it is recommended:
-
to use a secured incomer (UPS) when available in the switchboard
-
to connect it as upstream as possible in the switchboard near to the main circuit breaker
This method helps to limit the risk of power outage on these devices.
Rule SW3: Use one gateway per cubicle in partitioned switchboard.
Use one gateway per cubicle in partitioned switchboard to avoid wireless communication disturbances.
Rule SW4: Use one gateway for a maximum of three non-partitioned cubicles.
Use one gateway for a maximum of three non-partitioned cubicles with a maximum cubicle width of 0.7 meters, to avoid wireless communication disturbances.