DOCA0194EN-00

Wireless Channel Assignment Plan Definition

Each gateway is set to one wireless channel.

A wireless channel has a limited bandwidth and it depends upon:

  • the number of associated gateways and their paired wireless devices

  • the wireless communication periods set in each gateway

NOTE: If the bandwidth in a channel exceeds the limit, it can lead to wireless communication disturbances and communication issues in the PowerTag system.

The two objectives of the wireless channel assignment plan are:

  • to assign a channel (11 to 26) to each gateway, to balance communication loads and to avoid future communication.

  • to define the two wireless communication periods:

    • one for the energy sensors and control modules

    • one for the HeatTag sensors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?