Wireless Channel Assignment Procedure
|
Step |
Action |
|---|---|
|
1 |
Add all the panel in the layout of the zone (strictly follow the scale of the layout) and tag each panel with a label. |
|
2 |
Indicate a legend to identify the type of panel and to associate easily with the PowerTag system. |
|
3 |
Define the overlapped wireless channel using the wireless spectral analysis (refer to Rule WCAP2). |
|
4 |
Define one or two reserved wireless channels for future evolution (refer to Rule WCAP3). |
|
5 |
Define wireless channel for each gateway and associated wireless devices (refer to Rule WCAP4). |
|
6 |
Define the wireless communication periods for the PowerTag energy sensor, control modules, and HeatTag sensor (refer to Rule WCAP5). |